qn9080 flash memory for user

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

qn9080 flash memory for user

1,079 Views
jung-jin
Contributor II

Hello.

We are going to use the flash memory of QN9080 to store the product serial number.
The size to be used is within 100 bytes.

(1) Is it okay to use QN's flash for user purposes?
(2) Which memory address is allowed for user purposes? (ex 0x3107 0000 ? )

-----------------more info

I think I found a function suitable for reading and writing internal ROM memory.
- framework / Flash / External / Source / Eeprom_InternalFlash.c
- EEPROM_ReadData(), EEPROM_WriteData()

When tested with this function, the data is stored and read well.
Is it okay to read and write data to the internal ROM memory using this function?

Reards,

Jung-jin

Labels (1)
  • QN

0 Kudos
Reply
0 Replies