qn9080 flash memory for user

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

qn9080 flash memory for user

1,026 次查看
jung-jin
Contributor II

Hello.

We are going to use the flash memory of QN9080 to store the product serial number.
The size to be used is within 100 bytes.

(1) Is it okay to use QN's flash for user purposes?
(2) Which memory address is allowed for user purposes? (ex 0x3107 0000 ? )

-----------------more info

I think I found a function suitable for reading and writing internal ROM memory.
- framework / Flash / External / Source / Eeprom_InternalFlash.c
- EEPROM_ReadData(), EEPROM_WriteData()

When tested with this function, the data is stored and read well.
Is it okay to read and write data to the internal ROM memory using this function?

Reards,

Jung-jin

标签 (1)
  • QN

0 项奖励
回复
0 回复数