pn5180 documentation

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

pn5180 documentation

1,650 次查看
Splatspeed
Contributor II

i want to do a uart replacement with 2 of these devices, but i need application notes for doing this without your libraries with 2 powered devices. a flow chart of the messages sent to the NXP chip would be great to do this

 

thx in advance Sean

0 项奖励
回复
1 回复

1,645 次查看
KaiLi
NXP TechSupport
NXP TechSupport

Hello @Splatspeed 

If you don't want to use NXP library to develop, then two suggestions for reference:

1. Between Master and PN518 is the SPI interface, there is a standard SPI communication protocol, no special application description here. PN5180 datasheet is open source. For PN5180 Antenna design, you can refer AN11740.

2. Between PN518 and Tag, this application varies according to the tag. If it is NXP's tag, you can download the relevant development documents from the official website.

Best Regards,

Thanks,

kelly

0 项奖励
回复