pn5180 documentation

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

pn5180 documentation

1,649件の閲覧回数
Splatspeed
Contributor II

i want to do a uart replacement with 2 of these devices, but i need application notes for doing this without your libraries with 2 powered devices. a flow chart of the messages sent to the NXP chip would be great to do this

 

thx in advance Sean

0 件の賞賛
返信
1 返信

1,644件の閲覧回数
KaiLi
NXP TechSupport
NXP TechSupport

Hello @Splatspeed 

If you don't want to use NXP library to develop, then two suggestions for reference:

1. Between Master and PN518 is the SPI interface, there is a standard SPI communication protocol, no special application description here. PN5180 datasheet is open source. For PN5180 Antenna design, you can refer AN11740.

2. Between PN518 and Tag, this application varies according to the tag. If it is NXP's tag, you can download the relevant development documents from the official website.

Best Regards,

Thanks,

kelly

0 件の賞賛
返信