mkw36z512 can't program using Jlink SWD

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

mkw36z512 can't program using Jlink SWD

468 次查看
YoungMin
Contributor I

Hi team,
I'm developing firmware for the MKW36Z512 40-pin BLE using MCUXpressoIDE. On the development board, debugging works via LinkServer, but on the custom board, the hardware is set up for J-Link debugging. I tried debugging with J-Link, but it fails to recognize the IC.

I'm not very familiar with the hardware, but looking at the schematic, I noticed that the DCDC pin is not connected. Could this be the reason why J-Link is unable to detect the IC? If I'm doing something wrong, I’d appreciate it if you could let me know the correct approach.

 

here is some pictures, please check it.

feel free to notice something.

thank you in advance.

 

- MCU Circuit

YoungMin_3-1744300952658.png

-J-LINK Setting

YoungMin_1-1744300802060.png

- Error message

YoungMin_2-1744300889445.png

 

标签 (1)
标记 (2)
0 项奖励
回复
1 回复

419 次查看
sofiaurueta
NXP Employee
NXP Employee

Hello,

 

Hope you are doing well.

 

Based on the FRDM-KW36 schematic and FRDM-KW36 Minimum BoM Development Board User’s Guide, DCDC pins should be connected.

 

If you can check this community post, there is more information on pull up/down resistor recommendations for SWD on this post: Design Considerations for Debug

 

I would also recommend reviewing the connections in your custom board with the following documentation:

 

Best Regards,

Ana Sofia.

0 项奖励
回复