jn5169 autoreporting attribute

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

jn5169 autoreporting attribute

2,143件の閲覧回数
dmitryshelkovsk
Contributor II

Hi!

I try on the basis of JN-AN-1189 and tsHA_LightSensorDevice to make automatic sending of attributes.

End Device:

#define LIGHT_SENSOR_MINIMUM_MEASURED_VALUE                            0x0001
#define LIGHT_SENSOR_MAXIMUM_MEASURED_VALUE                            0x00FC
#define LIGHT_SENSOR_MINIMUM_REPORTABLE_CHANGE                         0x01

#define HA_NUMBER_OF_REPORTS                         2

void vAPP_ZCL_DeviceSpecific_Init(void)
{
    /* Initialise the strings in Basic */
    memcpy(sSensor.sBasicServerCluster.au8ManufacturerName, "1NXP", CLD_BAS_MANUF_NAME_SIZE);
    memcpy(sSensor.sBasicServerCluster.au8ModelIdentifier, "ZHA-OccupancySensor", CLD_BAS_MODEL_ID_SIZE);
    memcpy(sSensor.sBasicServerCluster.au8DateCode, "20141604", CLD_BAS_DATE_SIZE);
    memcpy(sSensor.sBasicServerCluster.au8SWBuildID, "4000-0001", CLD_BAS_SW_BUILD_SIZE);

    /* Initialise the attribute in illuminance Measurement */

    /* Initialise the attribute in illuminance Measurement */
    sSensor.sIlluminanceMeasurementServerCluster.u16MeasuredValue = 0;
    //sSensor.sIlluminanceMeasurementServerCluster.eLightSensorType = E_CLD_ILLMEAS_LST_CMOS;
    sSensor.sIlluminanceMeasurementServerCluster.u16MinMeasuredValue = LIGHT_SENSOR_MINIMUM_MEASURED_VALUE;
    sSensor.sIlluminanceMeasurementServerCluster.u16MaxMeasuredValue = LIGHT_SENSOR_MAXIMUM_MEASURED_VALUE;
}

PUBLIC void vMakeSupportedAttributesReportable(void)
{
    uint16 u16AttributeEnum;
    uint16 u16ClusterId;
    uint8 i;

    tsZCL_AttributeReportingConfigurationRecord*    psAttributeReportingConfigurationRecord;

    for(i=0;i<HA_NUMBER_OF_REPORTS;i++)
    {
        u16AttributeEnum=asSavedReports[i].sAttributeReportingConfigurationRecord.u16AttributeEnum;
        u16ClusterId= asSavedReports[i].u16ClusterID;
        psAttributeReportingConfigurationRecord = &(asSavedReports[i].sAttributeReportingConfigurationRecord);
        eZCL_SetReportableFlag(1,u16ClusterId, TRUE, FALSE,u16AttributeEnum);
        eZCL_CreateLocalReport(1,u16ClusterId,0,TRUE,psAttributeReportingConfigurationRecord);
    }
}


   .....

    asSavedReports[1].u16ClusterID=MEASUREMENT_AND_SENSING_CLUSTER_ID_ILLUMINANCE_MEASUREMENT;
    asSavedReports[1].sAttributeReportingConfigurationRecord.eAttributeDataType = E_ZCL_UINT16;
    asSavedReports[1].sAttributeReportingConfigurationRecord.u16AttributeEnum = E_CLD_ILLMEAS_ATTR_ID_MEASURED_VALUE;

    asSavedReports[1].sAttributeReportingConfigurationRecord.u16MaximumReportingInterval=LIGHT_SENSOR_MAXIMUM_MEASURED_VALUE;
    asSavedReports[1].sAttributeReportingConfigurationRecord.u16MinimumReportingInterval=LIGHT_SENSOR_MINIMUM_MEASURED_VALUE;

    asSavedReports[1].sAttributeReportingConfigurationRecord.u16TimeoutPeriodField=0; //0
    asSavedReports[1].sAttributeReportingConfigurationRecord.u8DirectionIsReceived=0; //0
    asSavedReports[1].sAttributeReportingConfigurationRecord.uAttributeReportableChange.zuint8ReportableChange=LIGHT_SENSOR_MINIMUM_REPORTABLE_CHANGE;

.....

In code for test change MeasuredValue

PUBLIC void vUpdateKeepAliveTimer(void)
{
te_SwitchState eSwitchState = eGetSwitchState();

if( (eSwitchState == LIGHT_CONTROL_MODE ) || (eSwitchState == INDIVIDUAL_CONTROL_MODE ) )
{
if( u8KeepAliveTime > 0 )
{
u8KeepAliveTime--;
sSensor.sIlluminanceMeasurementServerCluster.u16MeasuredValue = sSensor.sIlluminanceMeasurementServerCluster.u16MeasuredValue + 1;

But End Device not reporting attribute. Moreover, if I read attribute on gate:

devchange: 0x00158d0001833d77 260 1 { cid: 'msIlluminanceMeasurement', data: { measuredValue: 27 } }

What can I do wrong?

ラベル(2)
0 件の賞賛
返信
1 返信

1,936件の閲覧回数
dmitryshelkovsk
Contributor II

All work. SED sent attr report every 0x00FC.

After debug code I'll find answer. Clean project and rebuild + be sure vLoadDefaultConfigForReportable renew parameters.

Sorry for stuped question.