iBeacon + Connectable Peripheral with QN9080?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

iBeacon + Connectable Peripheral with QN9080?

1,774 Views
mike6789
Contributor I

Hi, 

I am wondering if I can use the QN9080 as an iBeacon as well as a peripheral to connect to from an iPhone. I am able to get the iBeacon working with the Beacon demo in the SDK -- but now I want to also connect to the QN9080 for data transfer. Is this possible with one chip? Or do I need two?

Thank you

Labels (2)
Tags (3)
0 Kudos
Reply
1 Reply

1,708 Views
Sebastian_Del_Rio
NXP Employee
NXP Employee

Hi Michael, I hope you're doing well!

 

There's currently no implementation for a Beacon + Connectable peripheral on one device example available, but it could be a possible implementation. First a connection event should have to be triggered, then the device could keep sending non-connectable advertising packets.

For reference, could you please take a look at the BLE Application Developer's Guide, in the following path for the SDK?:

<…\SDK_2.2.2_QN908XCDK\docs\wireless\Bluetooth\Bluetooth Low Energy Application Developers Guide.pdf>

 

Please let me know if you need any more information.

 

Take care, best regards,

Sebastian

0 Kudos
Reply