connect PX533 using libnfc in python

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

connect PX533 using libnfc in python

3,137件の閲覧回数
bartmuskala
Contributor I

I have ordered a DL533N reader based on the NXP PR533 chip.

I have installed all required libraries. I try to find the NFC reader on my raspberry Pi 400. No luck...

I keep getting a "No NFC device found" on nfc-list.
Using pn53x-tamashell I get "pn53x-tamashell: ERROR: Unable to open NFC device."

I don't know where to start honestly. Have been googling, chat gpting and the likes.

Thanks for your help.

0 件の賞賛
返信
4 返答(返信)

3,102件の閲覧回数
bartmuskala
Contributor I

Re-reading your remark, I was wondering whether there was another method to connect using Python on raspberry Pi? Libnfc was the option I believed to use, but if there are other options that you can provide this is also good. I need it to connect and to read data from the card. Thanks.

0 件の賞賛
返信

3,065件の閲覧回数
Fabian_R
NXP TechSupport
NXP TechSupport

Hello sir,

Unfortunately, we don't have any tool for Linux or based in Python that I can recommend. Although, you can use a PCSC tool that may suit your needs. Since the PR553 is a USB solution, the NXP IC should be able to interface through these commands.

Regarding the interest in signing an NDA, please take a look at the following FAQs: https://www.nxp.com/support/support/non-disclosure-agreement-faqs:NDA-FAQS

Best Regards,
Fabian
0 件の賞賛
返信

3,112件の閲覧回数
bartmuskala
Contributor I

I will contact them but am also open to sign an NDA and test the software as well. Thanks for your help. 

0 件の賞賛
返信

3,116件の閲覧回数
Fabian_R
NXP TechSupport
NXP TechSupport

Hello sir,

My recommendation is that please contact Digital Logic for further information since, PR533 is a USB-integrated solution but, the direct support for LibNFC inst directly supported by us. Is possible that the version of LibNFC you are using, requires some adjustments to the shell script provided by d-logic.

In case you are interested in testing the PR533, we do provide a product support package but, it requires you to sign an NDA with NXP for access to downloading it.

Still, I can't assure you that our provided software will fully work with the DL533N directly since, I'm not fully sure how it is built.

Best Regards,
Fabian
0 件の賞賛
返信