beacon package

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

beacon package

1,315 Views
zherlei
Contributor II

hardware:JN5169

software:zigbee 3.0  --- end device

The end device has been added the network built by coordinator. The end device will poll 250 milliseconds once. Sometime, the following phenonmena are as follows when I remove coordinator(poweroff).

zigbee_7.png

bag tool:Ubiqua Protocol Analyzer

The last beacon request is too long to come. This will result in a large amount of electricity consumption. 

How can I control the exception?

Tags (1)
0 Kudos
Reply
1 Reply

1,233 Views
mario_castaneda
NXP TechSupport
NXP TechSupport

Hi,

Remember The time Delta is the time interval between 2 captured packets, which is calculated based on the elapsed time from the previous packet regardless of its source network or channel. are the same device 0xDBB3 and the one that is sending the beacon request?

What is the application note that you are working on?

Mario

0 Kudos
Reply