Zigbee network without NFC

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Zigbee network without NFC

1,922件の閲覧回数
salewtg
Contributor I

Hi,

I am using JN516x-EK004 Evaluation Kit with JN5169 modules. I am trying to make a prototype with ZigBee network using the elements from the kit, but without NFC commissioning.

Is there any demo or example code that could be appropriate as a starting point? So far I failed to find one, or to modify the default supplied demo.

Thanks in advance!

Aleks

タグ(3)
0 件の賞賛
返信
1 返信

1,796件の閲覧回数
navdeepsinghgil
Contributor II

Hi,

1) Did you try looking into the JN-AN-1189 app note? It is similar to JN-AN-1221, but is meant for JN516x-EK001 kit and does not use NFC commissioning. It uses EZ-mode commissioning.

2) In the JN-AN-1221  doc they do mention that you can do commissioning without using NFC, but I have not gone into it very deeply yet.

0 件の賞賛
返信