Zigbee network without NFC

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Zigbee network without NFC

1,344 次查看
salewtg
Contributor I

Hi,

I am using JN516x-EK004 Evaluation Kit with JN5169 modules. I am trying to make a prototype with ZigBee network using the elements from the kit, but without NFC commissioning.

Is there any demo or example code that could be appropriate as a starting point? So far I failed to find one, or to modify the default supplied demo.

Thanks in advance!

Aleks

标记 (3)
0 项奖励
回复
1 回复

1,218 次查看
navdeepsinghgil
Contributor II

Hi,

1) Did you try looking into the JN-AN-1189 app note? It is similar to JN-AN-1221, but is meant for JN516x-EK001 kit and does not use NFC commissioning. It uses EZ-mode commissioning.

2) In the JN-AN-1221  doc they do mention that you can do commissioning without using NFC, but I have not gone into it very deeply yet.

0 项奖励
回复