Zigbee. MC1322x Sensor mode firmware download

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Zigbee. MC1322x Sensor mode firmware download

1,449 Views
rostislav
Contributor III

Hello everybody!

The Freescale toolkit has set of devices. One of them is "MC1322x Sensor mode" or another name "1322x SRB"

I am looking for the original firmware for 1322X SRB board. Where may I download the binary?

Thank you in advance.

Labels (1)
Tags (1)
0 Kudos
Reply
1 Reply

1,168 Views
jc_pacheco
NXP Employee
NXP Employee

Hello,

The demo binaries for each demo can be found under BeeKit installation path:

ZeD demo:

"C:\Program Files (x86)\Freescale\ZeD 1.6.5\Embedded"

Virtual Remote demo:

"C:\Program Files (x86)\Freescale\Virtual Remote\Embedded Images"

Weather Station:

"C:\Program Files (x86)\Freescale\Weather Station\Embedded Images"

You can load some demos using the BeeKit ARM7 xxx codebases.

Please keep in mind that MC1322x platform is already marked as EOL and not supported.

0 Kudos
Reply