Zigbee LightLink

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Zigbee LightLink

2,373件の閲覧回数
craigclark
Contributor I

Has anyone had any success in getting multiple controllers based on AN-1171 to connect via LightLink.  I can connect to multiple lighting devices fine, but I cannot get 2 controller to connect (the second one is factory new).

As per the instructions I am pressing the button to start the commissioning simultaneously on both (or as simultaneously as I can humanly achieve), but looking at the debug information, neither seem to see the requests from the other.

ラベル(1)
タグ(2)
0 件の賞賛
返信
1 返信

2,051件の閲覧回数
craigclark
Contributor I

Ok, further investigation says I am receiving the interpan data on the second (factory new) unit.

From the serial debug

ZCL_Task got event 22

& event 22 by definition is ZPS_EVENT_APS_INTERPAN_DATA_INDICATION

but nothing further happens, it appears to be thrown away in vZCL_HandleInterPanIndication

0 件の賞賛
返信