Zigbee LightLink

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Zigbee LightLink

2,336 Views
craigclark
Contributor I

Has anyone had any success in getting multiple controllers based on AN-1171 to connect via LightLink.  I can connect to multiple lighting devices fine, but I cannot get 2 controller to connect (the second one is factory new).

As per the instructions I am pressing the button to start the commissioning simultaneously on both (or as simultaneously as I can humanly achieve), but looking at the debug information, neither seem to see the requests from the other.

Labels (1)
Tags (2)
0 Kudos
Reply
1 Reply

2,014 Views
craigclark
Contributor I

Ok, further investigation says I am receiving the interpan data on the second (factory new) unit.

From the serial debug

ZCL_Task got event 22

& event 22 by definition is ZPS_EVENT_APS_INTERPAN_DATA_INDICATION

but nothing further happens, it appears to be thrown away in vZCL_HandleInterPanIndication

0 Kudos
Reply