Zigbee 1229 has errors every time it is compiled

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Zigbee 1229 has errors every time it is compiled

2,364件の閲覧回数
jun951753jun951
Contributor III

I used the 1229 to extract the 1229 zip to C:\NXP\bstudio_nxp\workspace。

There were no problems after the first Bulid all.But if I delete the project and import BUlid all again here, a lot of errors will occur.What should I do?

befor first  project ->Bulid all  pastedImage_1.png

after    project ->Bulid all 

pastedImage_2.png

If you delete a project and repeat the above operation, many errors will occur

project ->Bulid all 

pastedImage_3.png

What should I do to be free from mistakes?

ラベル(2)
0 件の賞賛
返信
3 返答(返信)

2,251件の閲覧回数
mario_castaneda
NXP TechSupport
NXP TechSupport

Hi,

Please look at the next community post https://community.nxp.com/docs/DOC-340028 

Regards,

Mario

0 件の賞賛
返信

2,251件の閲覧回数
jun951753jun951
Contributor III
  • Is the following picture normal after compilation?

  • pastedImage_1.png
  • But a lot of header files and variables, you can't see the definition.Will this affect future development?
  • pastedImage_2.png
0 件の賞賛
返信

2,251件の閲覧回数
mario_castaneda
NXP TechSupport
NXP TechSupport

Hi Juan,

Is the following picture normal after compilation?

Yes, As you can see, you generated the AN1229_ZBP_Coordinator_JN5169.bin

But a lot of header files and variables, you can't see the definition. Will this affect future development?

No, you must take as reference the console log.

Regards,

Mario