ZigBee Stop reporting attributes

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

ZigBee Stop reporting attributes

4,945 Views
randolfhu
Contributor III


Hi Sirs,

 

We are working on KW22. We set the Auto reporting of Humidity and Temperature every 1 minute by 4 steps, sending binding and the auto reporting timer value of Humidity and Temperature from ZC to ZED. After few hours testing, the ZED stop reporting. From the wireshark log, the wireshare log is in attachment, we found the short address - DCF3 sent the "permit join request" at 14:22:43.448 and successfully joined the network. After that, ZED keep sending Identify Query. Do you know why the ZED stop reporting?

 

 

2209102016-03-04 14:22:43.4489230xdcf3BroadcastZigBee ZDP62Permit Join Request

 

2209392016-03-04 14:22:43.9286830x00000xdcf3ZigBee ZDP61Permit Join Response, Status: Success

 

2210342016-03-04 14:22:48.5418030xdcf3BroadcastZigBee HA62ZCL Identify: Identify Query, Seq: 2

 

Platform: MKW24D512 Beekit: 3.0.2 Codebase: 4.0.1 Test Tool: 12.2.1

 

The Keys of this Zigbee network, FYI.

5A:69:67:42:65:65:41:6C:6C:69:61:6E:63:65:30:39 -Trust Center Link Key

b2:84:cf:69:b6:ba:dc:3b:f2:73:93:c6:97:31:49:26 -Network Key

 

Thanks,
Jake

Original Attachment has been moved to: BSP02.00stress-test_20160304.pcap.zip

Labels (2)
Tags (3)
0 Kudos
Reply
6 Replies

4,172 Views
drewgislason
Contributor I

One possibility (without seeing your over-the-air logs it's hard to tell) is that the EZ-Mode commissioning was unable to complete (hence the Identify Query). This could because you don't have matching clusters on the two nodes (that is and input cluster on the one node matching an output cluster on the other node). Reporting works through the binding table, which means it needs to complete that binding on the Reporting node.

0 Kudos
Reply

4,172 Views
jc_pacheco
NXP Employee
NXP Employee

Hello Jake, did you try the latest Kinetis BeeStack ZigBee Protocol Stack (REV 5.0.0)  ?

0 Kudos
Reply

4,172 Views
randolfhu
Contributor III

Hi Juan,

We are upgrading the ZigBee Protocol Stack Rev 5.00. Is it a known issue of old ZigBee release?

If the issue still can be reproduced on V5.00, what kind of logs should I provide to you?

Thanks,

Jake

0 Kudos
Reply

4,172 Views
jc_pacheco
NXP Employee
NXP Employee

I'm glad that you are upgrading to latest revision. Basically some issues were solved there, I'm not aware if this is included but either way the previous version is no longer supported.

If the issue is still present, please provide all sniffer logs and application behavior for us to reproduce in our evaluation boards.

0 Kudos
Reply

4,172 Views
randolfhu
Contributor III

Hi Juan,

Thanks for your response. We will keep reproducing it in the new release.

Thanks,

Jake

0 Kudos
Reply

4,172 Views
randolfhu
Contributor III

Hi

Is there any response or information. we found 4 out of 12 devices have the behavior. ZEDs stop reporting attributes before send the "permit join request" to ZC.

Thanks,

Jake

0 Kudos
Reply