ZigBee Endpoints Reserved

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

ZigBee Endpoints Reserved

9,553 Views
luisburgos
NXP Employee
NXP Employee

Endpoints are logical extensions added to a single ZigBee radio which permits support for multiple applications, addressed by the Endpoint number.

Endpoint Number can be anyone between 1 and 240.

There are two special endpoints: 0 and 255. Endpoint 0 is used for the configuration and management of the entire Zigbee devide. Through this endpoint, the application can communicate with other layers of the Zigbee stack to initialize and configure them. Attached to endpoint 0 is the Zigbee device object (ZDO). Endpoint 255 is used to broadcast to all endpoints, while endpoints 241-254 are reserved for special functions.

Refer Chapter 4 "Application Framework" of the Software Reference Manual for ZigBee attached.

Endpoint simple descriptor example:

const zbSimpleDescriptor_t Endpoint9_simpleDescriptor = {

  9, /* Endpoint number */

  0x4, 0x1, /* Application profile ID */

  0x0, 0x1, /* Application device ID */

  0, /* Application version ID */

  5, /* Number of input clusters */

  (uint8_t *) Endpoint9_InputClusterList, /* Input cluster list */

  0, /* Number of output clusters */

  (uint8_t *) Endpoint9_OutputClusterList, /* Output cluster list */

};


Labels (2)
0 Kudos
Reply
0 Replies