Wireless solution powered by coin cell battery

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Wireless solution powered by coin cell battery

2,015 Views
pepikas
Contributor I

Hello,

I would like to ask you about MRB-KW019032EU - 868 MHz with 32 MHz XTAL? Has somebody tried to power up this board or this mcu from coin cell battery? How long does it take to discharge the battery with sleep modes? Is the result time in years? Thank you.

Labels (1)
Tags (3)
0 Kudos
Reply
1 Reply

1,795 Views
EarlOrlando
Senior Contributor II

Hello Josef,

I recommend you to take a look into the MKW01 datasheet​ where you will find information about the supply voltage (minimum 1.8 V, table 9 "Transceiver recommended operating conditions") which will let you know if the desired battery would work for you.

pastedImage_1.png

Also, the datasheet shows information about the power consumption in the different sleep modes (table 10 "Power supply current") which is useful to calculate the time that your battery would have the MCU powered on.

pastedImage_2.png

Best regards,

Earl Orlando.

/* If this post answers your question please click the Correct Answer button. */

0 Kudos
Reply