WiFi Channel State Information (CSI) Extraction For RW612 eval board

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

WiFi Channel State Information (CSI) Extraction For RW612 eval board

1,310 Views
Sushant23
Contributor I

Dear Team,

I have a NXP RW612 Evaluation Board does it support WiFi CSI extraction in the 2.4 and 5 GHz band? If yes, is there any SDK code/Github sample code available?

Thanks,
Sushant

0 Kudos
Reply
2 Replies

1,246 Views
jimmychan
NXP TechSupport
NXP TechSupport

The CSI documents are under Documentation in "Secure" . So, require login and request it is needed approval.

RW612: Wireless MCU with Integrated Tri-radio: 1x1 Wi-Fi® 6 + Bluetooth® Low Energy 5.4 / 802.15.4 |...

 

 

0 Kudos
Reply

1,298 Views
James015Sims
Contributor I

Hello!

Information on explicit WiFi CSI extraction support for the NXP RW612 Evaluation Board in both 2.4 and 5 GHz bands is not readily available in standard documentation or initial search results. While the hardware likely has the capability, specific SDK code or GitHub samples aren't confirmed. To get a definitive answer and potential resources, consult the NXP Community Forum and directly contact NXP technical support, as they are the most reliable sources for this specific feature on the RW612.

0 Kudos
Reply