Why does Zigbee-3-0-Base-Device have two default input cluster

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Why does Zigbee-3-0-Base-Device have two default input cluster

1,666件の閲覧回数
18341265598
Contributor II

Hi everyone,

 

    In the app.zpscfg file of the project Zigbee-3-0-Base-Device, i discover that there have two 'default' input clusters and don't have any ‘default' output cluster, as below:

    pastedImage_1.png

    Do you know the reason is that.

    Thanks you very much.

ラベル(2)
0 件の賞賛
返信
1 返信

1,625件の閲覧回数
Sebastian_Del_Rio
NXP Employee
NXP Employee

Hi Zhang, I hope you're doing well!

 

Thank you for your feedback, it seems to be a mistake in the configuration. In the meantime, you can create a new Output Cluster with the same properties as your Default Input Cluster and delete the second Default Input Cluster.

 

Best regards,

Sebastian

0 件の賞賛
返信