Why does Zigbee-3-0-Base-Device have two default input cluster

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Why does Zigbee-3-0-Base-Device have two default input cluster

1,643 Views
18341265598
Contributor II

Hi everyone,

 

    In the app.zpscfg file of the project Zigbee-3-0-Base-Device, i discover that there have two 'default' input clusters and don't have any ‘default' output cluster, as below:

    pastedImage_1.png

    Do you know the reason is that.

    Thanks you very much.

Labels (2)
0 Kudos
Reply
1 Reply

1,602 Views
Sebastian_Del_Rio
NXP Employee
NXP Employee

Hi Zhang, I hope you're doing well!

 

Thank you for your feedback, it seems to be a mistake in the configuration. In the meantime, you can create a new Output Cluster with the same properties as your Default Input Cluster and delete the second Default Input Cluster.

 

Best regards,

Sebastian

0 Kudos
Reply