WLAN8101H Implementation Requirements

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

WLAN8101H Implementation Requirements

ソリューションへジャンプ
1,841件の閲覧回数
paulsons
Contributor I

Hello, and thank you for reviewing my post.

I am designing a small, high-speed, wireless sensing device to implement in my research. Our lab conducts impact experiments on various materials, collecting images at frame rates up to 10 MHz and strain data at sampling rates up to 100 MHz. For my device, I am scaling the sampling rate back to below 50 MSPS with an 8-bit ADC.

I am looking at using wifi as an IoT platform for the high throughput capacity. The location that this device will be used is in a well-shielded basement, so interference is low. I'm interested in the WLAN8101H front-end module for wifi 6 for its small footprint and the high throughput of wifi 6. Are there any recommended MCU or MPU devices to use with this product? From my understanding, the MCU/MPU will need to be able to output a TX signal to interface with the WLAN8101H. Are there other specific requirements in order to get the highest throughput out of the WLAN8101H?

0 件の賞賛
返信
1 解決策
1,826件の閲覧回数
vicentegomez
NXP TechSupport
NXP TechSupport

Please remember that the WLAN810H is only a front end module, maybe will be easier if you use one of our WiFi devices, this devices have support for some of our MCUs/MPUs using the MCUXpreso SDK, please check

 

https://www.nxp.com/products/wireless/wi-fi-plus-bluetooth:WIFI-BLUETOOTH

Maybe the IW620 or the 88W9098 can be a good option 

 

Regards

Vicente Gomez

 

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,827件の閲覧回数
vicentegomez
NXP TechSupport
NXP TechSupport

Please remember that the WLAN810H is only a front end module, maybe will be easier if you use one of our WiFi devices, this devices have support for some of our MCUs/MPUs using the MCUXpreso SDK, please check

 

https://www.nxp.com/products/wireless/wi-fi-plus-bluetooth:WIFI-BLUETOOTH

Maybe the IW620 or the 88W9098 can be a good option 

 

Regards

Vicente Gomez

 

0 件の賞賛
返信