Using multiple software timers

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Using multiple software timers

3,390 Views
netravatib
Contributor I

Hi All,

I am working on HAS application for JN516x series. I am facing problem with

timers.

Actually I want to use multiple(4) timers in my application, but when I am

starting my second timer on boot up module is printing fully junk data, and

it is getting hang also.

I am using these software timers of hardware counter based. May be I am

unable to keep count of my software timers running if I am correct.

So could you please help me to sort out this problem. And if I am getting

some examples for hardware timers also will be useful for me.

Thanks,

-Netravati

+91 8892853064

0 Kudos
Reply
2 Replies

3,226 Views
stephanie_m
NXP TechSupport
NXP TechSupport

Hello, 

You can find several application notes, other types of documents and software examples in the following links: 

It will depend on how are you managing them. Also, you should be careful that the stack it's not using the same timer as you do for other type of tasks.  

 

Best Regards, 

Estephania 

0 Kudos
Reply

3,225 Views
netravatib
Contributor I

Hi,

Thanks for your response.

But As explained in JN-UG-3075 JenOS user guide that Use of Tick Timer as Hardware Counter I have created and using my software timers. In that case if I am using more than 2 timers I am facing the problem which I explained in previous question.

So please let me know if any other document related to that or anything else need to be done.

Thanks,

Netravati B

0 Kudos
Reply