Use DBG_vPrintf() with IEEE 802.15.4 Application

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Use DBG_vPrintf() with IEEE 802.15.4 Application

2,189 次查看
ramonet
Contributor II

Hi, I simply trying to print into a terminal  using DBG_vPrint  I have tried so many combinations

but no matter what I cant get the uart to print into a terminal.

I am using a JN-5169 dongle with BeyondStudio.

And I modified the JN-AN-1174 template  (IEEE 802.15.4 Application Template for JN516x) end device file and makefile.

The files compile fine and the resulting bin can be loaded into the jn5169 dongle.

I attached these modified files to this message.

I am doing the print call in:

PUBLIC void AppColdStart(void)
{
/* Disable watchdog if enabled by default */
#ifdef WATCHDOG_ENABLED
vAHI_WatchdogStop();
#endif


vInitSystem();


DBG_vUartInit(DBG_E_UART_1, DBG_E_UART_BAUD_RATE_115200);

// vStartActiveScan();

while (1)
{

DBG_vPrintf(TRUE,"Hello");
// vProcessEventQueues();

}
}

The issue must be something related to my makefile or am I using this UART function incorrectly?

Any help would be much appreciated.

标签 (2)
1 回复

2,149 次查看
ramonet
Contributor II

The bug was in the makefile .

CFLAGS += -DDBG_ENABLED should come right after TRACE ?= 1

That and I disabled  DEBUG ?= HW