USB-KW24D512

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

USB-KW24D512

2,160件の閲覧回数
salah
Contributor III

Hi

I have 2 TWR-KW2x broad. For my experiment I need couple more. Can I use USB-KW24D512 as a TX, RX node instead buying another TWR-KW2x ? As an example if I would like to perform dual pan testing, as per instruction I am required 3 TWR-KW2x board to perform the demo. Can I use USB-KW24D512 instead ?

Any answer would be highly appreciated.

Thanks,
Salah

タグ(2)
1 返信

1,986件の閲覧回数
AngelC
Senior Contributor I

Dear Salah,

You could always use the USB-KW24D512 board to load BeeKit solutions. The Beekit new project’s wizard will let you choose the target board, including USB-KW24D512. Please just notice some demos will work differently since the dongle does not have some features such as many buttons, LEDs, etc. The same fact should be taken in consideration in case you want to develop a custom solution.

Regards,

AngelC