UART usage

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
3,107件の閲覧回数
lukaszgesieniec
Contributor II

Hi,

I want to communicate with another uC using UART. My application is based on thread_router_bluetooth_wireless_uart_hybrid example. Should I use SerialManager or FSCI module from Wireless Connectivity Framework? Any example?

Thanks

ラベル(3)
0 件の賞賛
返信
1 解決策
2,784件の閲覧回数
gerardo_rodriguez
NXP Employee
NXP Employee

Hello Lukasz,

The serial manager is used for communication to the upper layers in the stack. For most thread examples, the serial manager is user by the shell interface and communicates through UART to the OpenSDA MCU.

Since the KW41 only has one UART, you would need to disable the serial manager to have access to the UART. Once disabled, you can use the SDK drivers for the UART module. There are examples for this driver located in <SDK installation>\boards\frdmkw41z\driver_examples\lpuart\.

FSCI is a serial protocol used to control the Connectivity stack through serial commands.

Regards,

Gerardo

元の投稿で解決策を見る

1 返信
2,785件の閲覧回数
gerardo_rodriguez
NXP Employee
NXP Employee

Hello Lukasz,

The serial manager is used for communication to the upper layers in the stack. For most thread examples, the serial manager is user by the shell interface and communicates through UART to the OpenSDA MCU.

Since the KW41 only has one UART, you would need to disable the serial manager to have access to the UART. Once disabled, you can use the SDK drivers for the UART module. There are examples for this driver located in <SDK installation>\boards\frdmkw41z\driver_examples\lpuart\.

FSCI is a serial protocol used to control the Connectivity stack through serial commands.

Regards,

Gerardo