UART debug output on PNEV5180B

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

UART debug output on PNEV5180B

426件の閲覧回数
henry_pootle
Contributor I

I am trying to enable debug logs over UART on the evaluation board I have (PNEV5180B)

Unfortunately, I didn't find any schematics for the board, so I made some assumptions. The first one is that J201 is a UART port connected to the ARM MCU. Taking into account that it has 3 pins marked as TX, RX and Ground I think it is quite plausible. 

Then I've checked how the work with UART was implemented in lpcopen lpcxpresso SDK for lpc1769 and did the same. I managed to make all related IRQ triggers, and I believe smth is transferred, but I still can't manage to get any data on the pins themselves. They just keep silent (not noise, just silence). I've tried all 3 UARTs, they stay the same.

So the questions are:

   - Is J201 actually an UART?

   - Which UART port does it correspond to?

   - Are there any functional examples of using UART communication with PNEV5180B boards?

 

Thank you.

 

ラベル(1)
0 件の賞賛
返信
0 返答(返信)