Triangulation In Thread Network, is it possible?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Triangulation In Thread Network, is it possible?

1,724 Views
senizhuseyin
Contributor I

Hello,

   I would like to know if it is possible to achieve localization data of a mobile node via multilateration/trilateration/triangulation in Thread Network. I am new to 802.15.4. We have FRDM-KW41Z boards. As far as I read, triangulation is possible in a ZigBee network. I am now learning/working on Thread Network and checking Thread Demo applications in SDK_2.2_FRDM-KW41Z. I understand that in Thread network, an end device node can directly send message to only its parent router node. So I can not figure it out how to provide triangulation for a mobile end device. Is it possible?

Regards,

Seniz

Labels (2)
1 Reply

1,573 Views
haidong_zheng
NXP Employee
NXP Employee

Pure end device only could send packet to it's parent. But any REED device could store it's neighbors Link Margin information even when its role in Thread is a end device.