Thread Example Not working

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Thread Example Not working

2,905件の閲覧回数
pierslfx
Contributor I

Hello,

I am trying to get the thread host interface example working.

I have downloaded the SDK from Welcome to MCUXpresso | MCUXpresso Config Tools  and I am trying to run the frdmkw41z_wireless_examples_thread_host_controlled_device_freertos example. 

I have flashed it to my frdmkw41z board, which flashes the RGB LED blue. I connected a UART to USB adapter running on COM 4.

I downloaded the NXP Test Tool 12 to test out the THCI functionality. It recognizes the com port. Whenever I send a command, there is a TX entry but no RX response. If I plug the board in when its off, I can see a few RX commands as the board starts up.

Any help would be greatly appreciated.

0 件の賞賛
返信
3 返答(返信)

2,729件の閲覧回数
stephanie_m
NXP TechSupport
NXP TechSupport

Hello, 

To try to recreate your issue, could you please tell me which IDE are you using?

Best Regards,

Estephania  

0 件の賞賛
返信

2,729件の閲覧回数
pierslfx
Contributor I

Hello,

I am using the MCUXpresso IDE v10.0.2 [Build 411] [2017-07-11] .

Thank you in advance!

Piers

0 件の賞賛
返信

2,729件の閲覧回数
stephanie_m
NXP TechSupport
NXP TechSupport

Hello, 

I used the latest version available in the MCUXpresso web page, and I did not have any problem while working with the Test Tool. 

THR_hcd.PNG

Which baud rate are you using? 

Best Regards, 

Estephania 

0 件の賞賛
返信