The problem of receiving multicast data at multiple endpoints

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

The problem of receiving multicast data at multiple endpoints

1,518件の閲覧回数
zgmwork
Contributor II

Hi:

     I added two new dimmer endpoints to the JN-AN-1218-Zigbee-3-0-Light-Bulb routine, and then added all three endpoints to the same group ID. When sending data to this group ID, only two endpoints can receive data at the same time, and the other endpoint can not receive data. Is there restriction on the endpoint number receiving multicast data .

ラベル(1)
2 返答(返信)

1,447件の閲覧回数
mario_castaneda
NXP TechSupport
NXP TechSupport

Hi Guomiao,

There is no limitation. 

Is all the endpoint discoverable?

Did you capture the packets in the air? Do you have the sniffer log?

Regards,

Mario

0 件の賞賛
返信

1,447件の閲覧回数
zgmwork
Contributor II

 

Mario:

     I changed BDB_QUEUE_SIZE to 3 and it was normal. 

QQ图片20190725081946.png