The problem of receiving multicast data at multiple endpoints

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

The problem of receiving multicast data at multiple endpoints

1,512 次查看
zgmwork
Contributor II

Hi:

     I added two new dimmer endpoints to the JN-AN-1218-Zigbee-3-0-Light-Bulb routine, and then added all three endpoints to the same group ID. When sending data to this group ID, only two endpoints can receive data at the same time, and the other endpoint can not receive data. Is there restriction on the endpoint number receiving multicast data .

标签 (1)
2 回复数

1,441 次查看
mario_castaneda
NXP TechSupport
NXP TechSupport

Hi Guomiao,

There is no limitation. 

Is all the endpoint discoverable?

Did you capture the packets in the air? Do you have the sniffer log?

Regards,

Mario

0 项奖励
回复

1,441 次查看
zgmwork
Contributor II

 

Mario:

     I changed BDB_QUEUE_SIZE to 3 and it was normal. 

QQ图片20190725081946.png