* Test environment :
- JN5169
- SDK : JN-SW-4163
- device : Coordinator, Sleepy device
- JN-AN-1174
I am using vAppApiSaveMacSettings() before vAHI_Sleep(E_AHI_SLEEP_OSCON_RAMON) and vAppApiRestoreMacSettings() when AppWarmStart().
My problem is the following.
The mac seq number is always same if it transmits by vAppApiMcpsRequest() when sleepy device was woken from sleep mode .
That mac seq is 76.
But When none sleep, it's normally increase by one.
The attachment is sniffer log.
Best Regards,
lee
Hi Lee,
Please print the pu8Payload[0] value before you go to sleep. The sEndDeviceData.u8TxPacketSeqNb++ is increasing the sequence number.
Regards,
Mario
Hi Lee,
You must modify the MAC_Pib_s structure before sending the data.
uint8 u8Dsn;/**< macDSN attribute */
.
.
} MAC_Pib_s;
mac_pib_CombinedMac.h
s_psMacPib->u8Dsn= count++;Let me know your findings.
Mario
Hi Mario,
Thanks for your response.
I have tested, but the result is same. This mac seq is always 76.
The following is source code.
PRIVATE void vTransmitDataPacket(uint8 *pu8Data, uint8 u8Len, uint16 u16DestAdr)
{
MAC_McpsReqRsp_s sMcpsReqRsp;
MAC_McpsSyncCfm_s sMcpsSyncCfm;
uint8 *pu8Payload, i = 0;PRIVATE u8 count;
s_pvMac = pvAppApiGetMacHandle();
s_psMacPib = MAC_psPibGetHandle(s_pvMac);
s_psMacPib->u8Dsn = count++;/* Create frame transmission request */
sMcpsReqRsp.u8Type = MAC_MCPS_REQ_DATA;
sMcpsReqRsp.u8ParamLength = sizeof(MAC_McpsReqData_s);
/* Set handle so we can match confirmation to request */
sMcpsReqRsp.uParam.sReqData.u8Handle = 1;/* Use short address for source */
sMcpsReqRsp.uParam.sReqData.sFrame.sSrcAddr.u8AddrMode = 2;
sMcpsReqRsp.uParam.sReqData.sFrame.sSrcAddr.u16PanId = u16panid;
sMcpsReqRsp.uParam.sReqData.sFrame.sSrcAddr.uAddr.u16Short = u16id;
/* Use short address for destination */
sMcpsReqRsp.uParam.sReqData.sFrame.sDstAddr.u8AddrMode = 2;
sMcpsReqRsp.uParam.sReqData.sFrame.sDstAddr.u16PanId = u16panid;
sMcpsReqRsp.uParam.sReqData.sFrame.sDstAddr.uAddr.u16Short = u16DestAdr;/* Frame requires ack but not security, indirect transmit or GTS */
sMcpsReqRsp.uParam.sReqData.sFrame.u8TxOptions = 0;//MAC_TX_OPTION_ACK;pu8Payload = sMcpsReqRsp.uParam.sReqData.sFrame.au8Sdu;
for (i = 0; i < (u8Len); i++)
{
pu8Payload[i] = *pu8Data++;
}/* Set frame length */
sMcpsReqRsp.uParam.sReqData.sFrame.u8SduLength = i;/* Request transmit */
vAppApiMcpsRequest(&sMcpsReqRsp, &sMcpsSyncCfm);
}
Regards,
Lee
Hi Lee,
You should add the code out of the vTransmitDataPacket and before of it.
s_psMacPib->u8Dsn= count++;
vTransmitDataPacket(&TxData,9,TagVstemp.u16coordShortAdr);Please let me know your findings.
Regards,
Mario
Hi Lee Wonsoo,
How are you implementing the sleep mode?
PRIVATE MAC_Pib_s *s_psMacPib;
while (1)
{
vProcessEventQueues();
if(sEndDeviceData.eState == E_STATE_ASSOCIATED)
{
s_psMacPib->u8Dsn= count++;
DBG_vPrintf(TRUE,"s_psMacPib->u8Dsn 0%0d;\n",s_psMacPib->u8Dsn);
vTransmitDataPacket(&TxData,9,TagVstemp.u16coordShortAdr);
}
if(sEndDeviceData.eState == E_STATE_TX_END)
{
}
}Regards,
Mario
Hi Mario.
I found the Issues in Makefile.
Before
CFLAGS += -DENABLE_OPT_IN_MAKE
CFLAGS += -DENABLE_OPT_RFD
After
#CFLAGS += -DENABLE_OPT_IN_MAKE
#CFLAGS += -DENABLE_OPT_RFD
I have changed for sleepy device but It was the wrong setting.
Thank you for your support.
Regards,
Lee