The connection problem of the main host (handheld device) and the anchor point (sub-anchor point and

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

The connection problem of the main host (handheld device) and the anchor point (sub-anchor point and

1,337 次查看
liuyanfeng2
Contributor I

The main (handheld) and anchor points (sub-anchor points and main anchor points) of KW38.

Now what we need is for handheld device A to be able to connect to anchor point A. Now let's say that anchor point A is disconnected from handheld device A, and handheld device A can connect to anchor point B.

If I want to implement such a feature, what should I do?I did this by placing the anchor IRK in handheld device A.This is when handheld device A scans to anchor point A or anchor point B, which is connected to anchor point A or anchor point B.

But this is not the case.Handheld device A is just connected to the anchor IRK that holds the first location.

 

What can I do so that I can hold A (the IRK that holds anchor A and anchor B) and connect to anchor A or anchor B?

Tell me, guide me, thank you!

标签 (1)
0 项奖励
回复
1 回复

1,290 次查看
Ricardo_Zamora
NXP TechSupport
NXP TechSupport

Hello,

 

I sent you a private message.

 

Regards,

Ricardo

0 项奖励
回复