Starting Matter develop with W71 on mac with using vscode?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Starting Matter develop with W71 on mac with using vscode?

3,199 Views
frank-lin-Sunon
Contributor III

I am new on nxp wireless developing.
How to i starting Matter develop with W71 on mac with using vscode?

I first install "MCUXpresso for VS Code" and all thing in "MCUXpresso Installer".
After import NXP Matter repository v1.4.0. i click import example from repository trying to start matter develop. But i found that there doesn't application name and path for me to create a project. It just import hthe project (different from other sdk).
And not sure what to do next.

Labels (1)
0 Kudos
Reply
5 Replies

3,168 Views
frank-lin-Sunon
Contributor III

After automatically installing other SDKs, I can compile the project.
But it is hard for me to found out where's the project file(where i can do some modify). Is there any document for that?

0 Kudos
Reply

3,155 Views
jimmychan
NXP TechSupport
NXP TechSupport
0 Kudos
Reply

3,130 Views
frank-lin-Sunon
Contributor III

Hi jimmy,

I follow this link and can build the project.

Where is my application code to modify? I would like to do some change to the project but can't find place to modify.
Also, is there a way to "CREATE" a matter project not "IMPORT"? I need to create a project , change the project name and copy all file to folder when product development.

0 Kudos
Reply

3,117 Views
jimmychan
NXP TechSupport
NXP TechSupport
0 Kudos
Reply

3,101 Views
frank-lin-Sunon
Contributor III

Hi Jimmy,

You didn't get my point.
I had using vscode for many years, i'm not asking how to use vscode. I'm asking is there any document about nxp matter file architecture?

The attachment is the file I saw after importing. If there is no relevant document description, it will be a disaster for development. Can't find the codes and files I should be paying attention to.

0 Kudos
Reply