Software stack for KW01Z

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Software stack for KW01Z

2,648件の閲覧回数
jtpark
Contributor IV

Hello,

I’d like to adopt KW01Z series for AMI (Advanced Metering Infrastructure) application.

Our MAC standard is 802.15.4e, so I looked over your document EUF-IND-T0970 by Cyril Zarader of BD Microcontrollers EMEA – “Enabling the Internet of Things(IoT)

However I have some questions as below for evaluation

1. How I can get the S/W stack for below layer?

Flexible IP Stack overview.jpg 

 

When I installed KW01 Connectivity Software in Website, but I couldn’t find any s/w stack except PHY.

And I need 6TOP s/w stack also in order to drive TSCH, however I couldn’t check it.

2. KW01Z is too small flash memory size for our application, so I’d like to use additional NXP MCU.

It means I only use RF block of KW01Z and s/w stack will be loaded to additional MCU.

If I use additional MCU + KW01Z, can I get the S/W stack?

Flash and RAM memory.jpg

3. What is PPDU max size of KW01Z?

 

4. Are transceiver clock(32MHz) and MCU clock(48MHz) clocks needed to input differently?

or can I use one external clock?

 Thanks.

0 返答(返信)