SoC/TRx 2.4 GHz for bluetooth and proprietary protocols

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

SoC/TRx 2.4 GHz for bluetooth and proprietary protocols

跳至解决方案
3,903 次查看
tobiasike
Contributor I

Hi anyone.

I am looking for a hardware plattform (RF-TRx or Sytem on chip) for a bigger project, which can be act as an bluetooth (low energy)  node  -- and on the other hand can be configured to handle a simple proprietary protocoll  (without all  the BT features),  its for compatibility mode.  

both configurations are independent, so the are two different firmwares.

best regards / nice weekend

标签 (3)
标记 (3)
0 项奖励
回复
1 解答
3,532 次查看
TudorS_
NXP Employee
NXP Employee

The upcoming Kinetis KW41Z will feature (alongside the Bluetooth LE v4.2 capabilities) a generic FSK mode on top of which any proprietary protocol using FSK modulation in the 2.4 GHz band will be implementable.

在原帖中查看解决方案

0 项奖励
回复
4 回复数
3,533 次查看
TudorS_
NXP Employee
NXP Employee

The upcoming Kinetis KW41Z will feature (alongside the Bluetooth LE v4.2 capabilities) a generic FSK mode on top of which any proprietary protocol using FSK modulation in the 2.4 GHz band will be implementable.

0 项奖励
回复
3,532 次查看
tobiasike
Contributor I

Thank you very much,   its what i am looking for.

When the device will be available /released  ?

0 项奖励
回复
3,532 次查看
TudorS_
NXP Employee
NXP Employee

The target is early Q3 2016.

There are however alpha programs you can be part of for early access to the technology. Please contact NXP support for more information.

0 项奖励
回复
3,532 次查看
tobiasike
Contributor I

Thank you --  i pick this information for our hardware selection document.

is there a approx. price for the product available ( @ 1kuint) ?

.. or may there are some distributer having this SoC already inside linecard.

0 项奖励
回复