SoC/TRx 2.4 GHz for bluetooth and proprietary protocols

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

SoC/TRx 2.4 GHz for bluetooth and proprietary protocols

Jump to solution
4,157 Views
tobiasike
Contributor I

Hi anyone.

I am looking for a hardware plattform (RF-TRx or Sytem on chip) for a bigger project, which can be act as an bluetooth (low energy)  node  -- and on the other hand can be configured to handle a simple proprietary protocoll  (without all  the BT features),  its for compatibility mode.  

both configurations are independent, so the are two different firmwares.

best regards / nice weekend

Labels (3)
Tags (3)
0 Kudos
Reply
1 Solution
3,786 Views
TudorS_
NXP Employee
NXP Employee

The upcoming Kinetis KW41Z will feature (alongside the Bluetooth LE v4.2 capabilities) a generic FSK mode on top of which any proprietary protocol using FSK modulation in the 2.4 GHz band will be implementable.

View solution in original post

0 Kudos
Reply
4 Replies
3,787 Views
TudorS_
NXP Employee
NXP Employee

The upcoming Kinetis KW41Z will feature (alongside the Bluetooth LE v4.2 capabilities) a generic FSK mode on top of which any proprietary protocol using FSK modulation in the 2.4 GHz band will be implementable.

0 Kudos
Reply
3,786 Views
tobiasike
Contributor I

Thank you very much,   its what i am looking for.

When the device will be available /released  ?

0 Kudos
Reply
3,786 Views
TudorS_
NXP Employee
NXP Employee

The target is early Q3 2016.

There are however alpha programs you can be part of for early access to the technology. Please contact NXP support for more information.

0 Kudos
Reply
3,786 Views
tobiasike
Contributor I

Thank you --  i pick this information for our hardware selection document.

is there a approx. price for the product available ( @ 1kuint) ?

.. or may there are some distributer having this SoC already inside linecard.

0 Kudos
Reply