Setting of Tx Power for FRDM KW41Z Board using Test tool

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Setting of Tx Power for FRDM KW41Z Board using Test tool

1,479 Views
zeshanyousaf
Contributor I

Hi,

I set Tx power of my FRDM-KW41Z board using "Radio test" of "Test tool" as shown in Picture below. It is not clear that which hexadecimal value of power level (hex value: 0x00 to 0x3E) corresponds to which absolute power level (a value in dBm).

Thanks.

pastedImage_1.png

Labels (1)
0 Kudos
Reply
1 Reply

1,227 Views
vicentegomez
NXP TechSupport
NXP TechSupport

Hi Zeshan

The FRDM-KW41Z is on pre-produccion phase, because of this all the information about the freedom and the KW41 is only available through the FAE or sales person, please contact your FAE or sales to get more information.

Please let me know if you do not have one.

Regards

Vicente Gomez

0 Kudos
Reply