Setting TX power level in BLE Host stack has no effect on peak current

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Setting TX power level in BLE Host stack has no effect on peak current

跳至解决方案
2,640 次查看
arpad_toth
Contributor II

Hello,

Setting power level in "BLE Host stack QN9080DK MCUXpresso SDK 2.2.0" stack has NO effect on TX advertisement current level, with these two power level the peak current is still 0.9mA:

Gap_SetTxPowerLevel(0u, gTxPowerAdvChannel_c)
Gap_SetTxPowerLevel(255u, gTxPowerAdvChannel_c)

BleApp_GenericCallback(const gapGenericEvent_t* const pGenericEvent)
{
      switch(pGenericEvent->eventType)
      {
            case gInitializationComplete_c:
                  /* set TX power */
                  assert(Gap_SetTxPowerLevel(255u, gTxPowerAdvChannel_c) == gBleSuccess_c);
                  assert(Gap_SetTxPowerLevel(255u, gTxPowerConnChannel_c) == gBleSuccess_c);
                  break;
                  ...
            case gTxPowerLevelSetComplete_c:
                  /* this is called twice, break point stops here */
                  break;
}

Also RSSI on RX side doesn't seem to be correlating.

What am I doing wrong?

标签 (2)
标记 (3)
0 项奖励
回复
1 解答
2,379 次查看
estephania_mart
NXP TechSupport
NXP TechSupport

Hello ,

  The register that needs to be modified it's the ANA_CTRL0[PA_POWER], the  API to access this register is RF_SetTxPowerLevel(). It can be set between 0x00 (minimum -  -30dBm) and 0xFF (maximum - +2dBm). 

 

  By default this field is not touched, so it is set to 0x7F which corresponds to 0dBm. 

Regards,
Estephania

在原帖中查看解决方案

0 项奖励
回复
2 回复数
2,379 次查看
arpad_toth
Contributor II

Controller_SetTxPowerLevel() is not an active interface for QN908X.

0 项奖励
回复
2,380 次查看
estephania_mart
NXP TechSupport
NXP TechSupport

Hello ,

  The register that needs to be modified it's the ANA_CTRL0[PA_POWER], the  API to access this register is RF_SetTxPowerLevel(). It can be set between 0x00 (minimum -  -30dBm) and 0xFF (maximum - +2dBm). 

 

  By default this field is not touched, so it is set to 0x7F which corresponds to 0dBm. 

Regards,
Estephania

0 项奖励
回复