SLN-VIZNAS-IOT Connect to Raspberry Pi 4

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

SLN-VIZNAS-IOT Connect to Raspberry Pi 4

1,742 Views
Kuya_PJ686
Contributor I

I’m attempting to create a smart lock using the SLN-VIZNAS-IOT and a raspberry pi 4. How can I send the unlock signal (attempting do this in the form of text) from the facial recognition to the Raspberry Pi 4? I currently have the two connected through Bluetooth using the companion app and the SLN-VIZNAS-IOT is connected to the raspberry pi using the usb A to usb c cable. 

thanks 

0 Kudos
Reply
1 Reply

1,718 Views
jeremyzhou
NXP Employee
NXP Employee

Hi,
Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.
To be prudent, I'd like to confirm with you about the design purpose, whether you want the SLN-VIZNAS-IOT to send a "message" via the USB port after recognization completes.
Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply