SL3S1203_1213

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

SL3S1203_1213

1,769 次查看
lysayly
Contributor I

pastedImage_1.png

pastedImage_2.png

G2iL+ 这个系列的芯片,能实现类似硬件灭活RFID的功能吗,

我的需求是能重复使用,通过外部一个高低电平或者连接的通断控制电子标签的RF功能的启用和灭活。

Can the G2iL  series of chips achieve a function similar to hardware inactivation of RFID?
My requirement is to be able to reuse, through an external high and low level or the on-off of the connection to control the activation and disactivation of the RF function of the electronic tag.
0 项奖励
回复
1 回复

1,718 次查看
Kan_Li
NXP TechSupport
NXP TechSupport

Hi 烨 李 ,

This tag supports a 32-bit kill password to permanently disable the tag, but it is not recoverable, and it is not controlled externally via a GPIO pin. I am sorry but you can not use it for that purpose.

Have a great day,
Kan


-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 项奖励
回复