Running into hardfault when getting Thread Router in Hybrid App

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Running into hardfault when getting Thread Router in Hybrid App

3,406 次查看
joachimk
Contributor II

Hi,

I'm running hybrid app (ble + thread) on KW41z processor. Everytime when the module is getting into a thread router, the application is running into a hard fault. After a quick system reset (reboot) the kw41z is a regular thread router and works stable in this mode (as long it does not change the device role again).

Why does this happen? Are there any known quirks? Are there some hints, settings, etc. which I can do or modify to not run into a hard fault?

Thanks in advance.

标签 (3)
0 项奖励
回复
3 回复数

3,220 次查看
ovidiu_usturoi
NXP Employee
NXP Employee

Hi Joachim Keh,

Could you provide more details about the application:

- what release are you using and what is the application?

- are you using IAR or MCU Expresso?

Regards,

Ovidiu

0 项奖励
回复

3,220 次查看
joachimk
Contributor II

Hi Ovidiu,

I'm using Connectivity Framework 1.0.2 and Kinetis Design Studio 3.2.0.

The application is based on ble_thread_router_wireless_uart example project.

Is it recomendable to update to MCU xpresso Software?

Is there a newer Framework available?

Thanks in advance.

0 项奖励
回复

3,220 次查看
ovidiu_usturoi
NXP Employee
NXP Employee

Hi Joachim,

Yes, it is a new release from January this year running with MCU Expresso. 

SDK could be downloaded from the following link : https://mcuxpresso.nxp.com/en/select by selecting the right board.

For MCU Expresso here is a link for downloading: MCUXpresso IDE|NXP 

Let me know if you need more details

Regards,

Ovidiu

0 项奖励
回复