Rigado R41Z debug problem

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Rigado R41Z debug problem

2,684 次查看
wojtek_84
Contributor I

Hello,

I have Rigado R41Z development kit which is based on KW41Z. I have problems with running BLE examples from Kinetis KW41Z Connectivity Software under KDS 3.2. I can debug all driver examples and demo apps (e.g. bubble) but when I try to start debug session for BLE example (e.g. beacon) I get an error:

Error in final launch sequence
Failed to execute MI command:
-exec-run

Flashing works fine. Jlink is recognizing the boeard correctly.

I compered the debug configuration but I connt see any difference between BLE and none BLE examples.

I would appreciate any help. 

Regards.

标签 (1)
0 项奖励
回复
2 回复数

2,428 次查看
msjadem
Contributor I

Wojciech,

We noticed the same issue here at Rigado. 

Make sure to check for updates in KDS. If you receive an error like " Unable to read repository at https://gnuarmeclipse.sourceforge.net/updates/content.xml", you can still download that repository in a zip file and manually update.

Regards,

Kyla Marino

Rigado Support Engineer

0 项奖励
回复

2,428 次查看
pavel_krenek
NXP Employee
NXP Employee

Hi Wojciech,

first you would check low power mode settings. It looks after the programming the mcu goes to sleep mode and disconnect the debugger.

Best regards,

Pavel 

0 项奖励
回复