Replace with the same type function, an error happen

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Replace with the same type function, an error happen

3,027件の閲覧回数
964884134
Contributor I

As we see in the picture: when I try to change the function "....AsInitiator" and rebuilt the projet , an error happen .These two functions ,"....AsInitiator" and "....AsTarget" , should be the same type and on the same header file, why is there an error that can't find the object? Undefined Symbol ?

ラベル(4)
タグ(1)
0 件の賞賛
返信
1 返信

2,941件の閲覧回数
stephanie_m
NXP TechSupport
NXP TechSupport

Hello,

 

Could you please share with me the release version of the SDK you are using? I just downloaded the latest one and the latest AN1217, just changed that line just as you have it and everything builds correctly.

target build.png


Did you modify something else?

Regards, 

Estephania 

0 件の賞賛
返信