Regarding aw-nm191-uSD kit

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Regarding aw-nm191-uSD kit

ソリューションへジャンプ
3,235件の閲覧回数
vaibhavd
Contributor II

I am trying to connect my wifi to access point but i am getting below error in  the serial terminal after pressing the reset button 

my boards are MIMXRT1060- EVK and AW-NM191-uSD

Starting webconfig DEMO
[i] Trying to load data from mflash.
[i] Nothing stored yet
[i] Initializing WiFi connection...
[wifi_io] Error: Error in wlan_card_status()
[wifi_io] Error: Card timeout wlan_download_normal_fw:362
[wifi] Error: sd_wifi_init failed. status code -1
[wlcm] Error: wifi_init failed. status code -1

vaibhavd_0-1599030758954.png

 

0 件の賞賛
返信
1 解決策
3,232件の閲覧回数
laserhsu
NXP Employee
NXP Employee

suggest to terminate debug sessions and unplug Dut and restart again. 

元の投稿で解決策を見る

0 件の賞賛
返信
4 返答(返信)
3,233件の閲覧回数
laserhsu
NXP Employee
NXP Employee

suggest to terminate debug sessions and unplug Dut and restart again. 

0 件の賞賛
返信
3,228件の閲覧回数
vaibhavd
Contributor II

Yes , I have done this same step but same error is come

0 件の賞賛
返信
3,200件の閲覧回数
stephanie_m
NXP TechSupport
NXP TechSupport

Could you please make sure that you modified the module to use in the setting of the project ?


regards

3,194件の閲覧回数
vaibhavd
Contributor II

Thanks for your help, Due to module connection issue we got this error . now it is working properly 

0 件の賞賛
返信