Regarding aw-nm191-uSD kit

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Regarding aw-nm191-uSD kit

跳至解决方案
3,180 次查看
vaibhavd
Contributor II

I am trying to connect my wifi to access point but i am getting below error in  the serial terminal after pressing the reset button 

my boards are MIMXRT1060- EVK and AW-NM191-uSD

Starting webconfig DEMO
[i] Trying to load data from mflash.
[i] Nothing stored yet
[i] Initializing WiFi connection...
[wifi_io] Error: Error in wlan_card_status()
[wifi_io] Error: Card timeout wlan_download_normal_fw:362
[wifi] Error: sd_wifi_init failed. status code -1
[wlcm] Error: wifi_init failed. status code -1

vaibhavd_0-1599030758954.png

 

0 项奖励
回复
1 解答
3,177 次查看
laserhsu
NXP Employee
NXP Employee

suggest to terminate debug sessions and unplug Dut and restart again. 

在原帖中查看解决方案

0 项奖励
回复
4 回复数
3,178 次查看
laserhsu
NXP Employee
NXP Employee

suggest to terminate debug sessions and unplug Dut and restart again. 

0 项奖励
回复
3,173 次查看
vaibhavd
Contributor II

Yes , I have done this same step but same error is come

0 项奖励
回复
3,145 次查看
stephanie_m
NXP TechSupport
NXP TechSupport

Could you please make sure that you modified the module to use in the setting of the project ?


regards

3,139 次查看
vaibhavd
Contributor II

Thanks for your help, Due to module connection issue we got this error . now it is working properly 

0 项奖励
回复