Reading data from the zigbee module through USB.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Reading data from the zigbee module through USB.

1,731件の閲覧回数
kousikbarathwaj
Contributor I

Hello,

I am new to embedded environment. I am using NXP's zigbee module(JN5168) mounted on the mezzanine board. It has various sensors interfaced through I2C and FTDI chip for serial communication through USB.

The chips are programmed with beyond studio software.  We are able to form zigbee network with two modules (one as coordinator and one as end-device). We are sending sensor data from the end-device to the coordinator. The coordinator is connected to the linux machine through USB.  Now the data in the coordinator has to used by other application running on the linux machine.  How can we read the data from the coordinator through USB.

Thanks.

ラベル(1)
0 件の賞賛
返信
0 返答(返信)