Reading data from sensor with Ntag5 Link

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Reading data from sensor with Ntag5 Link

1,735 Views
Tomado
Contributor I

Hello NXP-Community,


I wanted to consult for a project I was aiming to develop.


I want to read data from the barometric sensor (i2c) without MCU with NTAG5 Link. What peripheral components are required for NTAG5 Link? Is there an example schematic?


Also, is it possible to perform data reading with the phone (NFC) by making changes on the "NTAG 5 Development kit Android application source code"?


In summary, can I read data from the sensor connected to NTAG5 Link via i2c without battery and without MCU, just by making configurations on Android App?


Best regards

0 Kudos
Reply
1 Reply

1,720 Views
fangfang
NXP TechSupport
NXP TechSupport

Hello @Tomado .

For your application please kindly refer to the vedio of the demo board for the ntag 5 link as the link.

URL:https://www.nxp.com/products/rfid-nfc/nfc-hf/nfc-tags-for-electronics/ntag-5-family-demo-kit:NTAG-5-...

And the schematic of the board as the link.

URL:https://www.nxp.com/docs/en/quick-reference-guide/NTAG5-DEMOKIT-QSG.pdf

Have a nice day.

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-----------------------------------------------------------------------------

0 Kudos
Reply