Questions about the compatibility between BeeStack and Z-Stack

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Questions about the compatibility between BeeStack and Z-Stack

1,995件の閲覧回数
zhaotian
Contributor I

Hi,

Dose anyone know whether the BeeStack of FSL is  compatible with the Z-Stack of IT.They are both based on the provisions by the Zigbee alliance,and if the can work well on the same LAN?

Thanks.

タグ(3)
0 件の賞賛
返信
1 返信

1,879件の閲覧回数
AngelC
Senior Contributor I

Dear Zhao,

I am not familiar with the TI’s solution, but both BeeStack and Z-Stack are ZigBee-certified and therefore they have been proven to interoperate properly. Nevertheless, care should be taken to use the same configuration in both vendors’ devices. Parameters such as security keys, network configuration, profile version, etc. are important  to achieve communication between with each other.

If you find any issues when combining both solutions please let us know here so we could give you further recommendations and help you in the process.

Best Regards,

AngelC