Question Regarding PN5180 Card Emulation and Tag Reader

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Question Regarding PN5180 Card Emulation and Tag Reader

3,569件の閲覧回数
tsotnek
Contributor II

Hello,

So this is the question for NXP support, can I use PN5180 as both Card Emulation and Tag Reader but not simultaneously. For example, if I combine HCE_T4T example and MIFARE Classic example. If I add another task and poll like 500ms for Phone and then 500ms for Mifare classic. Is it possible? I have tried it and it doesn't work I want to know if it's a problem on my side or it's impossible?

 

Thanks

3 返答(返信)

2,849件の閲覧回数
preethi_mh
Contributor I

Hi @tsotnek ,

 

Please  help me with this. or please direct me to any resources that can help.

 

Thanks,

Preethi

タグ(1)
0 件の賞賛
返信

3,517件の閲覧回数
Fabian_R
NXP TechSupport
NXP TechSupport

Thank you for submitting your question, we really appreciate your interest in our products.

The PN5180 IC is able to change its configurations without a RESET but, this isn't shown in any of our examples from the NFC Reader Library. My recommendation is that please explore the possibility of doing this without the library. In the next Application Note, AN12650 will guide you to use the PN5180 without a library.

Please check the  Datasheet commands (section), specially LOAD_RF_CONFIG and UPDATE_RF_CONFIG. These commands will manage the configuration changes that will be toggled while the application is running.

Unfortunately, the support for doing this is out of our scope.

I hope this information may have been useful.

Best Regards,
Fabian

2,853件の閲覧回数
preethi_mh
Contributor I

Hi @Fabian_R 

Need help ! 

I'm trying to do what @tsotnek is doing here. 

I understood the fact that I should try without Library first. I went through the application note you mentioned [AN12650]. But, In the documentation I couldn't find the Example code flow for the Card emulation mode. Can you please me with if you have example code for Card emulation here. 

Thanks,

Preethi

タグ(2)
0 件の賞賛
返信